LINAK Corporate Website - Linear Actuator Company LINAK.com Homepage

Applications

DESKLINE Applications

The DESKLINE® products, which conform to the most stringent safety regulations, can be used in many different applications. Beneath you will find some examples of where LINAK's products can be utilized:

Light office applications
Desks within the office sector where load capability is of less importance but characterised by a low noise level and high speed requirements.
The desks are mostly single column or 2 parallel systems.
You can choose between: DESKPOWER System.

Standard office applications
Standard office desks are standard workplaces, where space is needed and load not irrelevant. The desks are mostly equipped with min. 2 legs.
You can choose between: DL1DL5/DL6, DB5/DB6.

Special solutions
Examples of special solutions are receptions, info desks or e.g. a big CAD/CAM workstation. These solutions are often characterised by high demands in respect to performance.
You can choose between: DL1

Light industry applications
Applications within this area are often a kind of assembly or sorting desks, often where drawers or shelves are mounted on the application, setting high demands on load, stability etc.
You can choose between: DL1, DL2, LA31C 

Multi parallel office equipment
Some sit/stand applications are so large that they require several legs to be working in parallel. DESKLINE systems operate up to 16 legs in parallel. This goes for instance for large conference tables.
You can choose between: DL4/DB4, DL5/DL6, DB5/DB6
 

Speakers desk
As different persons require different heights on the speakers desk, all speakers should have the option of adjusting the height of the desk. Some might even want to sit down during the presentation, while others want to stand up.
You can choose between: DL2, DL4/DB4, DL5/DL6, DB5/DB6
 

Flat screen applications
As flat screens are becoming ever increasingly popular, a variety of applications for flat screens are seeing the light of day. Some applications, as the cabinet shown to the right, are meant to hide the TV away, only to be visible when needed....
 

...while others are for the sole purpose of adjusting the height of the flat screen as shown here.

A flat screen lifting system could consist of a DL4, DL9 or DL11 lifting column with a CBD4 or CBD5 control box and a DP1R infrared receiver with extension eye to receive the signal. Furthermore LINAK also offers the HB21F hand control for remote operation of the system
 

Leisure bed applications
Flat screens that can be raised and lowered into a bed frame is one of the latest applications that will revolutionize your bed room. When needed the flat screen can be raised out of the bed frame and lowered again when the TV is not needed. This feature solves many design issues in bed rooms and is at the same time a very convenient way of placing a TV in the room. The flat screen is exactly where you need it!

A system for this kind of application would normally be the same as for ordinary flat screens, illustrated above.

 

©2003-2008 LINAK Group. All rights reserved. Terms Of Use | Sitemap.